Technical FAQs

Ask a Question

Are the fuses on the front end of 8839 Altivar ATV66 used to protect the motor?

The fuses are used to protect the drive from short circuit. The drive has protective devise to protect the motor, such as ( Out Phase Loss, Motor overload, Current limit. )


CTA-ID : 7000
Was this helpful?
What can we do to improve the information ?