Technical FAQs

Ask a Question

Are the fuses required on the input of the Altivar ATV66 used to protect the motor?

No, the fuses are for short circuit protection of the drive. The drive has internal features for protection of the motor.

CTA-ID : 6999
Was this helpful?
What can we do to improve the information ?