Technical FAQs

Ask a Question

What can be done if the Altivar ATV56 unit is tripping on overvoltage on deceleration.

If only occurs when stopping may want increase the deceleration time and if necessary may need to install dynamic brake kit.


CTA-ID : 6710
Was this helpful?
What can we do to improve the information ?