Technical FAQs

Ask a Question

After the switch is unlocked on the ATV56 keypad, is there anything else to do to unlock the unit totally?

No, once the switch is unlocked the unit is unlocked--there is not an access lock menu on the ATV56.


CTA-ID : 6709
Was this helpful?
What can we do to improve the information ?