Technical FAQs

Ask a Question

Can he run the Altivar ATV56 drive without the motor and prevent it from tripping?

Yes. Go to menu 7.4 and then disable outphase loss.


CTA-ID : 6701
Was this helpful?
What can we do to improve the information ?