Technical FAQs

Ask a Question

What are the recommended cradle rejection pin keying for the cradle rejection kit for the Masterpact NW/NT?

A recommended cradle rejection pin keying chart for the drawout breaker is in the instruction bulletin provided with the NW breaker. Document number 48049-106-03 page 32.


CTA-ID : 6213
Was this helpful?
What can we do to improve the information ?