Technical FAQs

Ask a Question

What wire sizes can be used with the M9 C60H Circuit Breaker?

Cable range : pressure terminals are suitable for solid copper cables:
0.5 to 25A : 16mm^2 stranded or 25mm^2 solid
32 to 63A : 25mm^2 stranded or 35mm^2 solid


CTA-ID : 6250
Was this helpful?
What can we do to improve the information ?