Technical FAQs

Ask a Question

Can the Altistart ATS23 be used with Code F motor?

Issue:   Can the Altistart ATS23 be used with Code F motor?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   
Yes it can be used with Code F motor as long as the current rating is sized properly.


 
Was this helpful?
What can we do to improve the information ?