Technical FAQs

Ask a Question

Why does Altistart ATS23 only takes 2 or 3 seconds for the motor to come up to speed when the acceleration potentiometer is set to 14?

Issue:   Why does Altistart ATS23 only takes 2 or 3 seconds for the motor to come up to speed when the acceleration potentiometer is set to 14?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   The actual acceleration time may be different since they depend on load conditions, such as inertia and resistive torque.


 
Was this helpful?
What can we do to improve the information ?