Technical FAQs

Ask a Question

How is the zero current of the motor being detected on the Altistart ATS23?

Issue:   How is the zero current of the motor being detected on the Altistart ATS23?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   It is monitored through CT`s.


 
Was this helpful?
What can we do to improve the information ?