Technical FAQs

Ask a Question

Can customer replace the power terminal block with the blue plastic piece located at the top of the ATS23C15N unit where the line power comes in?

Issue:   Can customer replace the power terminal block with the blue plastic piece located at the top of the ATS23C15N unit where the line power comes in?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   No. No parts available. Replace starter with a current model..


 
Was this helpful?
What can we do to improve the information ?