Technical FAQs

Ask a Question

Does the Altistart ATS23 units have a problem with phase inversion if not wired up L1, L2 & L3 in order of if they were reversed?

The ATS23 would not have a problem w/ phase inversion for the power connections and it should still operate.


CTA-ID : 7303
Was this helpful?
What can we do to improve the information ?