Technical FAQs

Ask a Question

At what point will Altistart ATS23 unit trip after light is flashing indicating it is pulling more than 130%?

Issue:   At what point will Altistart ATS23 unit trip after light is flashing indicating it is pulling more than 130%?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Informed that this is a class 10 overload so looking at a table you see that at 150% it takes 90seconds, at 300% it takes 30sec & at 425% it takes 5 seconds so have to follow this.


 
Was this helpful?
What can we do to improve the information ?