Technical FAQs

Ask a Question

Can you run a second drive`s run command and speed reference from the first Altivar ATV66 drive performing master / slave operation?

You could use the NO contact of R2 relay set to running state to close LI2 to 24V. Could use the AO1 set to motor speed to AI2 and Com of the second drive for the speed reference. Make sure LI1 is jumpered to 24V on both drives.


CTA-ID : 6997
Was this helpful?
What can we do to improve the information ?