Technical FAQs

Ask a Question

What is the maximum humidity acceptable with the Altivar ATV66?

95% maximum without condensation or dripping water.


CTA-ID : 6996
Was this helpful?
What can we do to improve the information ?