Technical FAQs

Ask a Question

He has a 4-20ma signal in series to two Altivar ATV56 drives. Why does one drive operate at 87% speed and the other operate at 35% speed when have a 4 - 20ma signal tied in series on two ATV56 drives?

Need to make sure the voltage driver is strong enough for both drives.

CTA-ID : 6694
Was this helpful?
What can we do to improve the information ?