Technical FAQs

Ask a Question

Can you use Auto restart with outphase loss and do you need to cycle the run command to get it to run after the auto-restart attempt on an ATV56?

Auto restart will reset an output phase loss, if you have drive set up for 2 wire control and LI1 and LI2 are maintained high and a speed reference is present the unit will run.


CTA-ID : 6692
Was this helpful?
What can we do to improve the information ?