Technical FAQs

Ask a Question

Can the ATV56 drive be reset by a logic input?

Yes, in menu 7.4 have autoreset parameter and can assign the logic input to this that will reset the resetable faults


CTA-ID : 6683
Was this helpful?
What can we do to improve the information ?