Technical FAQs

Ask a Question

What range of wire sizes is suitable for the IEC 947-2 rated M9 DPN Circuit Breakers?

Cable range : pressure terminals are suitable for 16mm^2 solid copper cables


CTA-ID : 6245
Was this helpful?
What can we do to improve the information ?