Technical FAQs

Ask a Question

Will the Altistart ATS23 unit notice a single phase condition during running operation?

Issue:   Will the Altistart ATS23 unit notice a single phase condition during running operation?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   
The unit does not have single phase protection during running operation, the over load however should sense the rise in current due to the open or shorted winding.


 
Was this helpful?
What can we do to improve the information ?