Technical FAQs

Ask a Question

What is the part number of the A2 busbarr on the Altistart ATS23C10N so he could replace it?

Issue:   What is the part number of the A2 busbarr on the Altistart ATS23C10N so he could replace it?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Not a replacement part  replace starter with a currrent model
 
Was this helpful?
What can we do to improve the information ?