Technical FAQs

Ask a Question

Does the Altistart ATS23 have a run permissive input.

Issue:   Does the Altistart ATS23 have a run permissive input.
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   There is just a stop and run input and 24V supply You can use Stop as a run permissive on  2 wire control.


 
Was this helpful?
What can we do to improve the information ?