Technical FAQs

Ask a Question

Are the fault relays a dry set of contacts between terminals 27 and 28 on the Altistart ATS23?

Issue:   Are the fault relays a dry set of contacts between terminals 27 and 28 on the Altistart ATS23?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   Yes, those are dry contacts.


 
Was this helpful?
What can we do to improve the information ?