Technical FAQs

Ask a Question

Can the keypad of the Altivar ATV66 be programmed to display motor speed in RPM?

Yes. Under menu 4.1 can select motor speed and program it for the synchronous speed of the motor, 700, 900, 1200, 1800 or 3600 RPM.


CTA-ID : 6979
Was this helpful?
What can we do to improve the information ?