Technical FAQs

Ask a Question

What is the maximum length of control cable that can be used for the 24vdc run command on an Altivar ATV66 drive?

Can have voltage drop and noise issues beyond 300 feet. Can use an 115vac interposing relay if more distance required.


CTA-ID : 6977
Was this helpful?
What can we do to improve the information ?