Technical FAQs

Ask a Question

What does pollution degree mean and what pollution degree does the ATV66 meet?

The pollution degree determines the amount of voltage that can creep across foil run spacing of a printed circuit board and/or particulate matter the can fall on a printed circuit board. The ATV66 meets Pollution Degree 3 per NEMA ICS-1 and IEC 664-1.

CTA-ID : 6972
Was this helpful?
What can we do to improve the information ?