Technical FAQs

Ask a Question

Can we use the Altivar drive on a resistive heating bank or a non motor load?

No, A drive wants an inductive load and a resistive heating application is a resistive load. There are people that build resistive heating control, but is not a drive application.

The drives are designed and intended to be used with motors only.


CTA-ID : 6971
Was this helpful?
What can we do to improve the information ?