Technical FAQs

Ask a Question

How is the LO+ used on the ATV18?

Issue: How is the LO+ used on the ATV18?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: The LO+ is the supply to the logic output and only has to be jumpered to 24V if a logic output is needed or can bring in external 24v source by connecting positive side to LO+ and negative side to COM.


 
Was this helpful?
What can we do to improve the information ?