Technical FAQs

Ask a Question

Is there any way to give a logic input to tell the ATV18 drive not to sum between AI1 and AI2 but to switch from one speed reference to the other?

No, They will need to use a relay to electrically isolate the analog input and the com.

CTA-ID : 6669
Was this helpful?
What can we do to improve the information ?