Technical FAQs

Ask a Question

Should the Altistart ATS23 wired in a delta or wye configuration?

Issue:   Should the Altistart ATS23 wired in a delta or wye configuration?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   
A grounded delta would work. A wye connection only provides 58 % voltage and an open delta configuration could cause either overload conditions or phase faults.


 
Was this helpful?
What can we do to improve the information ?