Technical FAQs

Ask a Question

What is the part number for the Altistart ATS23 control module?

Issue:   What is the part number for the Altistart ATS23 control module?
 
Product Line:   ATS23
 
Environment:  All
 
Cause:   N/A
 
Resolution:   
The part number was VW3G231C24Q for all ratings of the standard unit and part number VW3GP231C24Q for all ratings of the pump version control module. Both are obsolete with no replacement


 
Was this helpful?
What can we do to improve the information ?