Technical FAQs

Ask a Question

How can you unlock the Altivar ATV66 drive to be able to get to all the parameters?

First, you need to put the switch on back of keypad in the unlocked position (lock looks like is open and is down position) and then In menu 10 in access lock parameter set it for total access.

With the unit not being told to run at this point should be able to access and change all the paramters.

CTA-ID : 6965
Was this helpful?
What can we do to improve the information ?