Technical FAQs

Ask a Question

What is the voltage rating of the IGBT`s for the ATV18 unit?

The IGBT`s are rated for at least 1200v but did see that 1600v devices were used but could not distinguish which component was used when.


CTA-ID : 6663
Was this helpful?
What can we do to improve the information ?