Technical FAQs

Ask a Question

Can you return to Factory Settings with the ATV18?

Issue: Can you return to Factory Settings with the ATV18?
 
Product Line: ATV18
 
Environment: All
 
Cause: N/A
 
Resolution: In order to return to factory settings, Set parameter FCS to Yes.


 
Was this helpful?
What can we do to improve the information ?