Technical FAQs

Ask a Question

What Mag-Gaurd disconnect is recommended for the 8636 Altistart ATS46?

Only the thermal magnetic breakers are recommended for customer use. If customer uses Mag-Gaurd, it voids UL and the customer would need approval.


CTA-ID : 7245
Was this helpful?
What can we do to improve the information ?