Technical FAQs

Ask a Question

Can a disconnect be used on the load side of an Altivar ATV66 drive?

Current spikes can be seen at the output of an ATV66 if the motor is disconnected when the drive is running, this can stress the IGBT`s and shorten their life.


CTA-ID : 6926
Was this helpful?
What can we do to improve the information ?