Technical FAQs

Ask a Question

What is included in a HOMVP14 Load Center Value Pack?

Issue:
Product design features

Product Line:
Homeline load centers

Environment:
Value Pack components

Cause:
Application

Resolution:
The HOMVP14 is Obsolete and replaced with the HOM3060M200PCVP (SEE FA232784 for components included in new value pack) 

The HOMVP14 included a HOM3040M200TC load center (with combination cover and equipment ground bar), 12 - HOM120, 1 - HOM230 and 1 - HOM250 branch circuit breakers.


CTA-ID : 6625
Was this helpful?
What can we do to improve the information ?