Technical FAQs

Ask a Question

Can the LH4N unit sense overload conditions during operation, after start-up?

The LH4N units do not provide overload protection. All they do is reduce voltage for ramp up and/or ramp down.


CTA-ID : 7534
Was this helpful?
What can we do to improve the information ?