Technical FAQs

Ask a Question

Does the softstop function in the LH4N slow the motor?

The softstop is not braking function. The voltage to the motor will be decreased over the deceleration time. This continues to provide forward torque to the motor. It is used to prevent sudden stops not to reduce motor speed.

CTA-ID : 7531
Was this helpful?
What can we do to improve the information ?