Technical FAQs

Ask a Question

What is the motor thermal state indicating on the Altivar ATV66 keypad display?

It is a percentage from 0-200%, 100% will cause the yellow LED on the face of the drive to blink as an early warning, when it reaches 118% the drive will trip on Motor Overload Fault.

CTA-ID : 6924
Was this helpful?
What can we do to improve the information ?