Technical FAQs

Ask a Question

Can the LH4N unit be bench tested without a load?

No. It must be connected to a load. If there is no load, the soft starter will not operate properly.


CTA-ID : 7515
Was this helpful?
What can we do to improve the information ?