Technical FAQs

Ask a Question

What does it mean in the catalog on page 3 where it states LH4N soft start must be used with Galvanic isolation to separate the soft start from the motor when the motor is not running. ?

This means that the LH4 need to be wired on the output side on a full voltage starter so than when it is off, there is no power on line terminals of the LH4.

CTA-ID : 7510
Was this helpful?
What can we do to improve the information ?