Technical FAQs

Ask a Question

Can the Altivar ATV66 standard drive accept an encoder feedback?

No but you can use a converter to convert encoder signal to a 0-10V or 4-20(0-20) ma and use it to control speed.


CTA-ID : 7208
Was this helpful?
What can we do to improve the information ?