Technical FAQs

Ask a Question

Would it be better to use wye or delta configuration when using Isolation transformer to step down from 575V line power to 460V to power an Altivar ATV66?

Told him the drive does not really care if it is wye or delta. Since wye configuration has more impedance, it probably would be a better choice. Make sure the system is properly grounded.


CTA-ID : 7207
Was this helpful?
What can we do to improve the information ?