Technical FAQs

Ask a Question

Are the analog outputs of the Altivar ATV66 self powered or are they loop powered from a remote source?

The 0-20mA is a self powered analog outputs.


CTA-ID : 7206
Was this helpful?
What can we do to improve the information ?