Technical FAQs

Ask a Question

Can you power a 4-20mA transducer from the Altivar ATV66 10V power supply?

No, the 10V is only good for 10mA. The 24V is good for 210mA then you must subtract 10mA for every logic input that you use. As long as the transducer does not exceed the available amperage, should be ok to use the 24V but be aware could damage power supply if get a short on external device.

CTA-ID : 7205
Was this helpful?
What can we do to improve the information ?