Technical FAQs

Ask a Question

Can you program the Altivar ATV66 unit with single phase and it retain the memory?

Need to remove the jumps on CL1 to L1 and CL2 to L2. Then power up CL1 and CL2 only. This will allow the programming be saved.


CTA-ID : 7203
Was this helpful?
What can we do to improve the information ?