Technical FAQs

Ask a Question

Has a QO230 breaker that has 2 clips on one of the bottom and only one on the other side. Is this correct?

Yes, the one clip is used to guide and hold the breaker to the mounting rail the other 2 are the bus connections.


CTA-ID : 5518
Was this helpful?
What can we do to improve the information ?