Technical FAQs

Ask a Question

What is the replacement On Off toggle part number for Class 2510 Type KW*?

Issue: What is the replacement On Off toggle part number for Class 2510 Type KW*?

Product Line: 2510 type K manual switches

Environment: Products sold and used in the United States

Cause: Replacement toggle, handle, on/off switch part number needed for the 2510 type KW manual switch

Resolution: 9998 HW1.

This applies to Class 2510 Types KW1A, KW1AH, KW1B, KW1BH, KW1H, KW2, KW2B, KW2BH, KW2C, KW2CH, KW2H, KW5, KW5A, KW5AH, KW5B, KW5BH, KW5H, KW6, KW6BH, KW6C, KW6CH, and KW6H switches.


CTA-ID : 4417
Was this helpful?
What can we do to improve the information ?