Technical FAQs

Ask a Question

What wire binding torque should be applied to the NC100H Multi 9 supplementary protector lugs?

10 to 40 A: #18 to #2 AWG (1 to 35 mm^2 )cables; torque 31 lb-in. (3.5 Nm)
50 to 80 A: #8 to #1 AWG (1 to 50 mm^2 )cables; torque 49 lb-in. (5.5 Nm)


CTA-ID : 6183
Was this helpful?
What can we do to improve the information ?